Limit
Limit the instrument's output setting to prevent damage to the load caused by operator error.
| AC Voltage | Set the maximum voltage. |
| DC Voltage | Set the minimum and maximum voltages. |
| Current |
Current limits are set for all or individual phases. You can set the maximum current as well as the positive and negative peak currents. |
| Frequency | Set the minimum and maximum frequency. |